Contact us at Sales@sugatsune.com or (800)-562-5267. *If you are calling from Canada, please call at 310-329-6373.

LIN-X1000
Red Dot Award
Demonstration of LIN-X1000

What is the Red Dot Award?


Established in 1955, the Red Dot Award is decided by the Design Zentrum Nordrhein Westfalen in Essen, Germany. The award features products which have been released in the last two years and recognized for being outsanding. This year, over 5500 products were submitted from 54 different countries. Products are judged by international specialists who appraise the functions, innovativeness, quality amongst 9 different standards. Along with the iF Design Award and the International Design Excellence Awards, it is one of the 3 biggest design awards in the world.

What is the LIN-X1000?


Sugatsune's Lateral Door Opening System Series opens and closes flat and parallel to the wall. It features Sugatsune's Motion Design Tech, opening in unique ways with a soft close.

Features of the LIN-X1000


Works with Larger Doors

Works with doors up to 1100mm in width (accessible space is 900mm) meaning that wheelchairs can pass through.

LIN-X1000 Feature One

Opens with a Small Radius

Compared to regular doors, requires approximately 1/2 the space to open and close.

LIN-X1000 Feature Two

Closes Softly and Quietly

Has a damper which causes the door to close quietly. (The damper has 5 different adjustable levels of force).

LIN-X1000 Feature Three

Works with Heavier Doors: Up to 90kg

Has the weight bearing capacity to be used at boutiques, restaurants, office storage areas, and walk-in closets.

LIN-X1000 Feature Four

Reduces Time Required for Installation

Consists only of a lower arm, cover section and connecting bar. Those are the only components required during installation. It can be adjusted in 4 different directions: Up/down, left/right, backwards/forwards and the angle.

LIN-X1000 Feature Two

Many Possible Opening Styles

Can function as a single door, a parallel opening pair, a sideways opening pair, or as an L corner opening.

LIN-X1000 Feature Three

LIN-X1000 Specifications


This item is able to handle doors that are much larger than any other in its product series. It is capable of working with doors with widths up to 1100mm, with a largest opening width of 900mm, it can be used in areas where wheelchairs access. The largest height of door it can be used with is 2980mm. The LIN-X1000 is capable of being used with doors with a weight of up to 90kg. It has a built in damper which causes the door to close silently even if the door is heavier. Because the opening radius is approximately half of a regular hinge, it can be used in narrower spaces. It also has fewer parts than conventional items, making it much easier to install.

What is Motion Design Tech?


Motion Design Tech is Sugatsune's product lineup that features five different kinds of special motion. The idea behind this is that designs should not only be beautiful but should also have fantastic functionality that makes people's lives easier and more convenient. The basic motivation behind this series is "improving the feeling of motion", "installation convenience", and "convenient angles and radii". These ideas have been combined to produce the various features of this series. The movements are broadly broken down to:
  • Soft Motion
  • Free-Stop Motion
  • Power Assist Motion
  • Click Motion
  • Unique Motion

Other Awards and Recognition


The LIN-X1000 also won the Good Design Award in 2016. The Good Design Award is widely recognized and has been awarded to high qualities products since 1957.
Good Design Award

LIN-X Series and Related Product Catalogues


Product Lineup
MonoFlat LIN-X
MONOFLAT
LIN-X HINGE
LIN-X1000
LIN-X1000
MonoFlat LIN-X
MONOFLAT
LIN-X HINGE
LIN-X450,600
MonoFlat FAD
MONOFLAT FAD
(FOR PARTITION USE)
FAD-54
MonoFlat FAD
MONOFLAT FAD
(FOR LARGE SIZE CABINET)
FAD-44
MonoFlat FAD
MONOFLAT FAD
(FOR MEDIUM SIZE CABINET)
FAD-20
h
MonoFlat FAD
MONOFLAT FAD
(FOR SMALL SIZE CABINET)
FAD-5

subscribe to our newsletter