Innovation - Sugatsune
Free-Stop Motion
Stops At Any Angle
Soft-Motion
Quiet & Safe
Assist Motion
Lifts & Opens Easily
Click Motion
Click To Stop
Multi-Linear Motion
Controlled & Seamless
Unique Motion
Innovative Openings
Motion Design Tech is Sugatsune’s unique product design concept to provide specialized movement solutions. Operability of doors or lids can be improved by incorporating the 5 types of motion in the work environment. It can also improve ergonomics and efficiency of work that involves routine opening and closing movements, increasing the added value of the device and equipment.
SOFT MOTION
Sugatsune’s LapCon lid stays are ideal for a variety of cabinet applications, storage under bench seating, and information terminals. The lid stay arm holds the panel in place when in use, and will softly self-close when pushed shut. This is a perfect solution for quiet environments, and eliminates pinched fingers.
Disk dampers are suitable for foodservice applications, such as those for self-serve bakery cases or for candy. If the flap is pushed down slightly, it will close naturally and slowly by itself, without the need to lower by hand.
FREE-STOP MOTION
Torque hinges can be adjusted and left at any angle, creating convenience for the user:
1) Holds lid open without additional support hardware, minimizing additional support hardware
2) Lid won’t slam shut, increasing user safety and reducing equipment damage
Torque hinges can be used in a variety of monitor applications to hold the display at a steady angle. Applications include everyday uses such as multiple-monitor arrays, for screens on industrial equipment, and with payment terminals.
ASSIST MOTION
Lift assist hardware options enable users to lift large or bulky lids with a fraction of the energy they would otherwise need. Especially useful for industrial equipment or appliances.
CLICK MOTION
Detent hinge hardware “clicks” between set positions at various angles, and holds panels open at the set position. User is confident that the panel is secure by the clicking motion.
UNIQUE MOTION
Sugatsune’s LIN-X (“links”) laterally-opening hardware was created to open doors in a shallow radius, without obstructing the space in front of the cabinet. Unique solution for kitchen islands, retail storage in narrow spaces, and industrial equipment access panels.
MULTI-LINEAR MOTION
Can be used for conveyor guide positioning units and workpiece extrusion units.
Enables smooth position adjustments while supporting the guide bar and can be installed in narrow spaces where conventional linear guides could not be implemented.