Add a Premium to Interior Spaces by Using Sliding Doors on Linear Motion Rails
Posted On Sep 5th 2023
Posted On Sep 5th 2023
Posted On Sep 5th 2023
Today we are looking at linear motion guide rails of the kind used on many of our sliding door systems.
When you want to elevate the user experience of a space, one of the most powerful and cost-effective measures you can take is to use better hardware solutions for common applications.
One excellent example of this is the use of sliding doors. They are uncommon compared to swinging doors and, therefore, a bit exotic, which makes them visually intriguing. By ensuring that your sliding doors are also easy to use and a pleasure to operate, you can give the end user a luxurious, memorable experience.
Linear motion rails facilitate back-and-forth linear movement for carriage systems. Just like a railroad car on the train track, there are only two ways that a carriage on a guide rail can go: along the rail in one direction or along the rail in the opposite direction. This maintains the alignment of the carriages, ensuring smooth, precise, consistent movement.
Guide rails have extensive industrial applications but can also be used architecturally—as we do at Sugatsune America. The guide rails in our door systems mount easily onto ceilings and (where applicable) floors, ensuring secure carriage placement from which doors can be hung. These doors will exhibit easy, whisper-quiet motion when slid open or shut.
Let’s look at some of the sliding door systems in our catalog that use linear motion rails.
Earned a High-Quality Product Design Award at Interzum 2023! | The trick of the MFU1200 is that its linear motion rails have a bend at the end, which is how the flush doors move out of the way of the wall when opened. Doors that use the MFU1200 don’t need handles to be installed, though you can add them if you desire. The movement is so smooth and easy that the user needs to simply push the doors softly to open them and pull on them gently to close. |
MFU1200 linear motion guide rails are:
Achieve perfect symmetrical motion when opening and closing sliding doors with the SDR-RA80SYN Synchronized Sliding Door System. The linear motion rails on this system are connected so that the carriages on each door move together.
Synchronized movement is incredibly clean and aesthetically pleasing. It’s also nice that the user only has to operate one door (if desired) in order to move both of them. The movement is light to the touch and as easy to use as a single door.
SDR-RA80SYN linear motion guide rails are:
For a classic, streamlined application of linear motion rails, the LM-80 Self-Closing Sliding Door System offers pure simplicity in form and function, as well as in installation. Doors hung on this system close all by themselves using gravity: The linear motion guide rails are very slightly inclined—just enough so that the door will close by itself while still being easy to open back up again.
This system is perfectly suited for anyone who wants to replace a traditional swinging door with a self-closing sliding door instead. They make a nice addition to upscale homes, conference rooms, and offices and are also well-suited for medical and institutional settings and some hospitality applications, where the self-close feature is highly convenient.
The LM-80 system is available in two variants: the regular LM-80 for use with most doors and the LM-80G for use with glass doors.
LM-80 linear motion rails are:
The linear guide rails used in these sliding door systems and others in our catalog share in common a goal of being useful to project managers, architects, and others in many different circumstances. You can hang all kinds of different doors on these systems, and in many cases, we have heavy-duty models so that you can hang even some of the heaviest doors.
Whichever doors you install with these systems, the linear motion provided through the guide rails will make them smooth-sliding, quiet, and very satisfying to use.
That’s it for today in the Sugatsune America Hardware Blog, but check out other blog articles for more resources, or look up where to buy our products.
If you have any unanswered questions, don’t hesitate to contact us. We would love to hear from you.
CAD files are available on each product’s detail page. Click the “CAD/BIM Files” tab, located in the middle of the page to download the different formats. If CAD files are not available for a specific component, please contact our Support Team
Toll Free: (800) 562-5267 (U.S.A. only)