Sugatsune America, Inc. Features Universal Designs at HD Expo, The Hospitality Design Event May 3-5, 2017.
Posted On Apr 26th 2019
Posted On Apr 26th 2019
Showcasing a variety of Modern Door Hardware Solutions at Booth #3074, Including Red Dot Award-Winning Product LIN-X1000
April 27, 2017 – Carson, Calif. Sugatsune offers high-quality products developed around universal design and is proud to be a part of the 2017 Hospitality Design Event. The company represents solutions for those architects and designers incorporating modern design, easy motion, and space-saving ideas into the hospitality industry — including modern door hardware. At this year’s HD Expo, Sugatsune is pleased to showcase several innovative hospitality industry design trends and universal design products, including the Red Dot award-winning LIN-X1000.
Red Dot Award Winner: LIN-X1000 Lateral Door Opening SystemThis Sugatsune modern door hardware was designed to provide smooth movement with a soft-close feature that operates on large doors weighing up to 200-lbs. It provides 4-way adjustability to ensure a flush, clean look when closed. The LIN-X-1000 allows doors up to 43 5/16” wide to swing open in a small radius, making it a great application for custom pantry doors, storage rooms, or other applications where there is a space constraint. |
[caption id="attachment_33861" align="aligncenter" width="280"] Sugatsune’s award-winning LIN-X1000 lateral door opening system.[/caption] |
[caption id="attachment_33862" align="aligncenter" width="300"] Synchronized Sliding Door Hardware SDR-RA80SYN[/caption] |
SDR-RA80SYN Soft Close Synchronized Sliding Door HardwareThe SDR-RA80SYN is a synchronized modern door hardware setup that doesn’t intrude into living or working areas. This unique system features double rollers with ball bearings and provides quiet precision movement as well as a soft-close system in both opening and closing directions. |
For those who want to see more modern door hardware and universal design products, visit booth #3074 to check out these hospitality industry design trends and many other precision-engineered solutions. Visitors will find everything from Sugatsune’s Fastmount panel mounting system and products that feature the latest soft-close technology to a comprehensive line-up of stainless steel crafted handles, pulls, and hooks.
With a heritage dating back to 1930, Sugatsune was established in America in 1982. ISO 9001 certified, the company has a rich tradition of manufacturing and distributing Japanese-quality hardware centered around universal design. Sugatsune America stocks over 6,000 unique parts in the U.S. to provide the highest level of service and convenience for architects, designers, and contractors.
LAMP® is a registered trademark of Sugatsune Kogyo, Inc. For more information, visit www.sugatsune.com. Connect with Sugatsune America via Facebook (facebook.com/sugatsune) and Twitter (twitter.com/sugatsune).
North American Headquarters:
18101 Savarona Way Carson, CA 90746 Tel: 310.329.6373, 800.562.5267 (USA only) Email: sales@sugatsune.com
Chicago Showroom / Sales Office:
121 W. Wacker Drive #1007 Chicago, IL 60601 Tel: 312.461.1081 Email: chicagoshowroom@sugatsune.com
CAD files are available on each product’s detail page. Click the “CAD/BIM Files” tab, located in the middle of the page to download the different formats. If CAD files are not available for a specific component, please contact our Support Team
Toll Free: (800) 562-5267 (U.S.A. only)