Sugatsune America Opens New Showroom Location in Chicago Loop and Will Host an Exclusive Grand Opening Event April 19th, 2017
Posted On Apr 10th 2017
Posted On Apr 10th 2017
Celebrating an evening with some of Chicago’s talented architects, designers, and builders – By Invitation Only
April 11, 2017 – Chicago, IL. Sugatsune America is pleased to announce the opening of their new Sugatsune Architectural Hardware Showroom located in the Chicago Loop, the vibrant heart of downtown Chicago. The new interior design showroom will feature the breadth and depth of their innovative hardware and showcase how it can be incorporated into modernized designs, with an emphasis on hardware for showroom kitchen cabinets. Co-hosting the Grand Opening event will be LUXE Interior + Design Magazine. This exclusive event will take place on Wednesday, April 19th from 5 – 8 pm at 121 W. Wacker Dr. suite 1007 with showroom tours, cocktails, and hors d'oeuvres to be served.
“The decision to expand our presence into Chicago’s central downtown location was a logical step in our business strategy,” said Steve Hirasawa, Executive Vice President of Sugatsune America. “The area is rich with diverse talent in interior design and architecture and this new location will make it convenient for them to see, feel and understand Sugatsune’s product line up.”
The showroom concept was developed to show the application of Sugatsune’s hardware, including innovative lateral opening cabinet systems. These systems are featured in a beautiful customized kitchen designed by leading residential design-build firm Benvenuti and Stein of Evanston, IL. These premium showroom kitchen cabinets are one of the focal points of the new interior design showroom.
Along with these universal design applied systems, the Sugatsune Architectural Hardware Showroom also features Sugatsune’s new synchronized sliding door system, its award-winning 3-way adjustable concealed hinges, and much more! Not only will this interior design showroom create an environment for architects and designers to come and get a feel for Sugatsune’s high-end premium hardware, but it will also serve as a great location to hold CEU events, lunch and learns, and private parties for the architectural and design community.
For more information on the Sugatsune Architectural Hardware Showroom Showroom, including the showroom kitchen cabinet hardware, event opportunities, and other inquiries, please contact us! Jenna Shaffer at 312-461-1081 or j.shaffer@sugatsune.com.
With a heritage dating back to 1930 and established in 1982, Sugatsune America Inc. is ISO 9001:2015 certified and has a rich tradition of manufacturing and distributing Japanese quality hardware, designed around universal design. Sugatsune America stocks over 6,000 unique parts in the U.S. to provide the highest level of service.
LAMP® is a registered trademark of Sugatsune Kogyo, Inc.
CAD files are available on each product’s detail page. Click the “CAD/BIM Files” tab, located in the middle of the page to download the different formats. If CAD files are not available for a specific component, please contact our Support Team
Toll Free: (800) 562-5267 (U.S.A. only)