Universal Design
Posted On Jun 14th 2021
Posted On Jun 14th 2021
Posted On Jun 14th 2021
When we speak about Aging in Place, we usually only think about the elderly or when we reference ADA compliancy, we are thinking only about accessibility for those with disabilities. It is true that over the next couple of decades, the U.S. will have over 85 Million people over the age of 65 and it is estimated that 1 in 8 Americans are challenged with disabilities. Both cohorts will play an important role in designing spaces. But why should we stop there? During a recent LivABLE Environment Conference, founder Linda Kafka stated that “everyone is temporarily abled.” When you think about it, it is true. At some point in our lives, we have or will need some assistance with everyday tasks whether it is because we grow old, have an unfortunate accident, or have people in our homes that need help. Even children would benefit from a “design and composition of an environment that can be accessed, understood and used to the greatest extent possible by all people regardless of their age, size, ability or disability.” Yes, we are speaking about Universal Design.
There are 7 key principals that Universal Design requires which are:
When designing Universal Design spaces, accessibility and safety are at the top of the list to consider. This means that layout and clearance could be the best starting point. If we put ourselves in the seat of someone bound to a wheelchair, pathways could be designed so that there is a minimum of 48” clearance and considerations should be given to 60” needed to turn around in a wheelchair. Not only would this make a space more accessible it would create a modern, more open aesthetic. Also, sliding doors could be incorporated to increase accessible while maximizing space. Best of all it ensures that if left open, the door will not impede on traffic areas. Adequate lighting is also critical. As we age, it is said that we need 30% more lighting to see the same thing we did when we were younger. And not just for performing tasks, but to ensure that we see transitions and other hazards that may pose a danger. Furthermore, minimizing stairs and/or eliminating thresholds to showers will also reduce functional barriers and safety risks.
Universal Design can also minimize stress even when performing everyday tasks. For example, in conversations about designing for the aging, we often hear the phrase “eyes to the thighs” referring to the sweet spot where it is most comfortable to reach and maintain balance when performing tasks. For the interior designer, this means ensuring that common access to cabinets and drawers occur in this area. Good solutions for storage are to maximize lower cabinet spaces and designing in islands with ample storage so people would not have to reach above their heads to reach several upper cabinets. But wouldn’t this be a good thing for everyone? Minimizing upper cabinets can even provide more space for windows that would allow in more light making the area look more spacious as well as lively.CAD files are available on each product’s detail page. Click the “CAD/BIM Files” tab, located in the middle of the page to download the different formats. If CAD files are not available for a specific component, please contact our Support Team
Toll Free: (800) 562-5267 (U.S.A. only)